AnsweredAssumed Answered

Did E8362B USB port work when daisy chain of USB hub is use?

Question asked by htlaw on May 18, 2006
Latest reply on May 19, 2006 by daras
Below is the method how the USB hub is daisy chain.

1) Input USB of 4 USB hub is connected to one of the USB port Of E8362B.
2) Then input USB of a 7 USB hub is connected to one out of 4 USB port on the 4 USB hub.
3) Then input USB of another 7 USB hub is connected to one out of 7 USB port on the 7 USB hub.
4) A ECal Module is connected to one out of 7 USB port on the 7 USB hub.

Do you think the E8362B  will still able to detect and communicated to the ECal Module? There will be 12 Ecal module connected on this daisy chain connection. The above setup is for customer testing purpose.  

Outcomes