AnsweredAssumed Answered

e8361 Sweep

Question asked by mclaughlinbryan on Nov 29, 2006
Latest reply on Nov 29, 2006 by Dr_joel
I am trying to perform an average over 3 samples and have two windows, each with 1 channel active.  My old 8722 swept both windows (and averages) simultaneously.  Thus, i had a 2 second sweep time averaged 3 times for a total of 6 seconds.  It seems the e8361 sweeps through window 1 and then window 2 synchronously.  When averaging factor of 3 is applied, it takes 12 seconds to perform the same measurements.  I have tried performing both measurements in the same window which seems to work but the display scale is wrong.  any thoughts on how to perform the measurements for both windows in parallel is appreciated.
bryan  

Outcomes