AnsweredAssumed Answered

Intuilink and 8720 - Can I allow user to plot data?

Question asked by JoeO'Neil on Dec 10, 2007
Latest reply on Mar 11, 2008 by odanzy
I am using the Agilent Intuilik software with Agilent's 82357B USB/GPIB Interface to control an 8720D VNA.

I am using the Intuilink "Connect to Network Analyzer" and "Get Data" function in Excel to capture trance information for a post processing calculation on an 8 way power divider. The post processing is done with VBA in Excel.

However, after capturing the data I need to release control back to the VNA so the operator can plot each piece of trace data on an 7550A graphics plotter.

Is it possible to pass the control back and forth between the VNA and the PC or do I need to find another work around?  

Outcomes