AnsweredAssumed Answered

Calibration: 85070E with ECAL Module

Question asked by Danhen on Jun 9, 2009
Latest reply on Jun 23, 2009 by Danhen
Greetings,
Dear Mr Agilent technical support.

First thank you for all the support that has been offered.


There were some questions regarding the process of calibration of application 85070E, the ECAL (N4691-60004) in this system. That is, the ECAL connected between the probe and network analyzer.


Ran the process of calibration standard. But in the short steps and water, images on the screen of the network analyzer (E5070B) were completely different from the screens displayed when the ECAL was not present.

Please Note:
ECAL not connected to the system

Screen of the Calibration Standard Short (without ECAL)
Image

Help 85070E
Image

Screen calibration standard in water (without ECAL)
Image

Help 85070E
Image



ECAL connected to the system

Screen in the default Short Calibration (with ECAL)
Image

Screen calibration standard in water (with ECAL)
Image

The questions are:
Considering the ECAL connected to the system, such as whether the calibration is correct?


When the ECAL is connected, what should the screens displayed by E5070B (Short patterns and water) during the calibration (85070E)?



Now, I thank all the attention

Daniel

(Electronics Technician / Student of Electrical Engineering)  

Outcomes