AnsweredAssumed Answered

85032F cal kit coefficients

Question asked by Tisfurs on Apr 20, 2009
Latest reply on Apr 22, 2009 by odanzy
I was reviewing the coefficients for this kit at Agilent's site and I noticed that two different delay values are given for the OPENS.  Which one is the male and which is the female?  Also, the disk with the kit, which says it is for the 8753 & 8720 series, has 41.03 for standard definition 2, and 40.74 for standard definition 8, but the F/W information in my 8722ES has 41.19 for both.  Which is correct?  

Outcomes