AnsweredAssumed Answered

GGB probes calibration

Question asked by cmwong on Nov 11, 2009
Latest reply on Nov 13, 2009 by odanzy
Hi,

I would like to perform a calibration for my 2-port GGB probes from my 4-port PNA. I am using an ISS substrate for my calibration. However, I am not sure if the 2-port Test Set needs to be physically disconnected from the 2-port PNA as the jumpers are still connected between both sets. Previously, I am also using GPIB and USB adaptor that was connected to the PNA and PC.

As such I would like to know what should be the exact connection for the calibration of the 2 port GGB probes.

current version of my PLTS is version 5.002.

Can anyone advice?

Thanks very much in advance.  

Outcomes