AnsweredAssumed Answered

Receiver Display with Booster Amp

Question asked by BrianR on Mar 9, 2006
Latest reply on Mar 16, 2006 by Dr_joel
I'm having trouble doing and E-Cal (using 85093C) with the power at the DUT set to 15dBm.  I keep getting and E-Cal orientation error.  The E-Cal works fine at 10dBm with the Booster set up but not +15dBm.

One thing I noticed is that Receiver Display reports that the power level at R1 is +5dBm but is measured to be -17dBm.

Is the receiver display R1 Trace accurate when using an external booster amplifier (see app note 1408-10 figure 8 for typical set up)?  

Outcomes