AnsweredAssumed Answered

Using Source power calibration with Scalar Mixer Cal

Question asked by SteveE on Apr 24, 2006
Latest reply on Apr 27, 2006 by gfarrel
I went to the trouble of writing some VEE functions to upload and download the source power flatness correction tables for the PNA so that I could get flat -20dBm power into my downconverting DUT. But now it appears that when I do a scalar mixer cal using the PNA calibration wizard the power flatness correction gets turned off. Is there a way to keep it on during the scalar mixer cal and ensuing measurements? Or can I do the calibration without it on and then be able to turn it on after the cal is complete and still get valid measurements?

Thanks for any help you can provide,  

Outcomes