AnsweredAssumed Answered

ENA TRL calibration

Question asked by mchsskrw on Apr 6, 2006
Latest reply on Apr 17, 2006 by mmule54
Can anyone tell me if the two port TRL calibration on the E5071B (Firmware Rev 6.01) is full TRL including switch reflection or is TRL* without correction for switch reflection.

The reason I ask is that during the TRL calibration, I don't see any measurements of switch reflection for the Line or Thru standards. The display only shows the four S parameters, unlike the 8510 which for the Line and Thru standards displays the four S parameters and the forward and reverse switch reflections during calibration.  

Outcomes