AnsweredAssumed Answered

Power calibration on the E5071B

Question asked by GW on Aug 4, 2006
Latest reply on Aug 4, 2006 by odanzy
I need to test a multi-octave up/down converter so I got a hold of an E4418B power meter to to a source power calibration. The analyzer could not find the power meter (address 13) so I got out the book and discovered that the only calibration setup shown utilizes an external USB to GPIB converter (which I don't have). Is there any way to use the GPIB port on the back of the unit (the power meter is now connected to this)?  

Outcomes