AnsweredAssumed Answered

Source power calibration

Question asked by wgifford on Apr 26, 2007
Latest reply on Jan 16, 2008 by Dr_joel
Hello,

I would like to perform a source power calibration, where the PNA (E8362B) and the power meter (N1911A) are connected via LAN.

The power meter and PNA are set up on the same network, and I have added the power meter as a LAN device in the Agilent Connection Expert (testing this connection in the Agilent connection expert was successful).

On the PNA, when I do System->Configure->Power Meter Settings... what should I use for a GPIB address so that the PNA finds the power meter?

Any suggestions are appreciated.

Thanks,
Wes  

Outcomes