AnsweredAssumed Answered

E5080A/B Changing Display During Calibration

Question asked by Paul55 on Dec 5, 2020
Latest reply on Jan 14, 2021 by s.wood

When performing the calibration from our software, I like to be able to set the display up so that the user can see if the calibration standard has been connected correctly.

 

Unlike any other analyzer I've used, it doesn't seem to be possible to change the display once the cal has been started, or even sweep a measurement on another channel.

 

eg:

SENSe1:CORRection:COLLect:METHod SPARSOLT
SENSe1:CORRection:COLLect STAN1

 

At this point, I'd like to somehow set the display to show Phase S11 and S22 (in separate windows) and be sweeping, but it doesn't seem to be possible, prior to executing the next line

 

SENSe1:CORRection:COLLect STAN2


Is there any work-around for this?

Outcomes