AnsweredAssumed Answered

How do I get an E36233A to retain static IP Address settings during several hours not connected to AC power?

Question asked by HamiltonWoods on Oct 21, 2020

I have two E36233A power supplies that I have configured with static IP Addresses. The IP Addresses persist through a disconnect from AC power for several seconds. However, two nights in a row I disconnected from AC power and the next morning one and then the other of the power supplies behaved like I do - it couldn't remember anything. Are there any suggestions other than, "Just don't disconnect from AC power."?

 

Thanks for your help.

Outcomes