AnsweredAssumed Answered

IO Libraries Draining Laptop Battery

Question asked by Paul55 on Oct 5, 2020
Latest reply on Oct 6, 2020 by Paul55

Has anyone else had battery drain issues with a laptop after installing IO Libraries?

 

I'm seeing this on 2 different Lenovo Thinkpads running Windows 10, and using the latest version of the IO Libraries.

 

Once the IO Libraries have been fully installed, the remaining battery time reduces by about 50%. Un-installing it, and all the IVI modules, returns the battery usage to normal.

Outcomes