Hello
Why it taking so long to load each DAQ to BanchVue.
I am using 5 DAQ and each of them required between 2 to 3 minutes to be loaded. What holding this program?
I do not think the PC is nigh be an issue.
I am running BanchVue 2019 on 64 bit Window 10 PC with Core I5 and 16 GB memory an solid state HD.
Any body have an idea why the loading of hardware in BanchVue is so slow and if there is a way to improve the speed?
Regards.
mirek
Try turning on IO Monitor using Connection Expert. Watch the IO traffic as you start up the DAQs and see if there are any timeout or other errors.
If you are using an 82357A/B USB-GPIB adapter, avoid the use of GPIB addresses 9,11,13,25,27 or 29.
If you have NI VISA and Keysight IO Library Suite, uninstall VISA Shared Components and then do a repair on Keysight IO Library Suite, which will install a fresh copy.
Try not to use RS-232 to USB adapters. They are very slow.
Brian