AnsweredAssumed Answered

34970A reading resistance on PNA

Question asked by toby10ant on Jul 16, 2020

I'm trying to record the resistance value of a thermistor on a PNA. When I send the command "MEAS:RES? (@103)" it's returning a difference value to what I see on the front of the instrument using monitor command. Do I need to configure a setting or is the number format different?

 

Cheers, Toby

Outcomes