Hello, I have encountering issue on DGN report. The DGN report is just show simple report only, exp. Module 2 slot 11a FAILED. I want to see details report as below sample:
Test 2348, Subtest 0, Module 3, Slot 1 FAILED.
Module power supplies -PPM(-10 V)
Low Limit : -1.05021500E+01
Result expected : -1.00000000E+01
High Limit : -9.49805100E+00
Result Received : -1.59754345E+01 Volts
I was trying to setup the DGN report option, but does not effect on displayed report.
Thanks,
Supriyanto
Supriyanto,
I believe you need to have an active Diagnostics Advanced Reporting license to get the report you are looking for. You can look this up in Kornshell using "codeword" and looking to see what licenses are active on your system.
Thanks,
Ben