AnsweredAssumed Answered

SCPI command to clear limit table

Question asked by yjames_1 on Jan 19, 2011
Latest reply on Jan 19, 2011 by yjames_1
Hi,

I've encountered a problem when tried to clear the limit table in VEE using command ":CALC1:LIM:DATA 0", there was a error message “Numeric data not allowed” shown on NWA. But sometimes it worked successfully.
The NWA is E5070B with firmware revision A.06.50. As the command works sometime, so I think it shouldn't be the problem of the old firmware revision.
Can any help me on this?
Thanks a lot!  

Outcomes