Hello,
at the moment I'm working with two AWG: M8190A from Keysight and each has two channels. I want to use them in dynamic Mode and one of them as a Primary and the other one as a Secondary. In general I just want to have two sequences and switch between them dynamically.
I'm just able to address the Primary AWG through the dynamic in Port.
Here is my questions:
How can I choose which Channel is addressed through the dynamic in Port (1 or 2)
How can I Start a Sequences which needs both AWGs and all Channels though the dynamic control of just one Channel of my Primary AWG ?
Thanks for the help in advance