I did not see a dedicated area for Keysight's Command Expert so I will try here. I have loaded Command Expert 2019 (Build 1.9.34) and I am trying to install a New Instrument. It sees all the instruments, connected via USB, and states downloading the SCPI Command Sets but terminates with an error. Could not load file or assembly 'Ivi.Visa.Interop,......
I am running IO Libraries 18.1.24715.0, Windows 10 1909. My guess its a Windows issue. Can anyone point me in the correct direction.
Thanks,
JoeD
Hi JoeD,
I think some of the IVI.org installation packages like IVI Shared Components or VISA Shared Component may not have have been installed successfully or got corrupted at some point.
Can you run the log gathering .exe attached and send me the .zip file it generates. I can take a look at it to determine the best next steps.
Thanks,
Vicnesh