Hello,
We're building out our VNA setup using M9010A PXIe Chassis. Is it possible to use NI PXIe-8301 Thunderbolt 3 controller to control the cards on the Keysight M9010A PXIe Chassis? In particular, we would like to use Keysight standard software to access M9375A PXI Vector Network Analyzer on the chassis via NI's Thunderbolt 3 controller. Do we know if this is possible? Thanks
I reached out to one of our PXI system compatibility experts and was able to ascertain the following information:
so it sounds like it may work fine with your PXIe chassis, but if you encounter problem number 2 above, you may have to wait until a fix is issued. The list of officially supported controllers and PCs can be found here: Tested Computer List.
If you need to further assistance on this issue, your best bet is to contact Keysight Support.