AnsweredAssumed Answered

TightVNC viewer connection error with E5071C VNA

Question asked by Alvarez001 on Apr 20, 2020

Hi all,

 

I am currently using tightVNC viewer for remote access to a VNA and am running into a connection error. The first time I ran the program and entered the IP address the viewer connected fine to the VNA with no problem. However after I try to log back in into the viewer I get an error window with following message: A connection attempt failed because the connected party did not properly respond after a period of time, or established connection failed because connected host has failed to respond. As of right now I have port forwarding on ports 5800 and 5900 and the firewall on VNA is turned off and I am not using a password for tightVNC. This is the IP address type that I am using 71.XXX.XXX.XXX::5900. Are there any suggestions or solutions that someone can recommend.

 

Thanks.

 

 

Outcomes