Hi,
I am new to de-embedding. I got s-parameter of a Twinax cable and same connector at the two ends of the cable from the manufacturer. They won't provide any s-parameter file only with the Twinax cable without connector. But for specific reason I need the s-parameter file only for cable w/o connectors. I found out de-embedding technique yesterday. Most of the de-embedding techniques as I found are removing the fixture which is in my case the connectors. But the s-parameter I got includes connector+cable. How to de-embed in this case in ADS?
There is de-embed component in ADS which takes s-parameter. What type of data should I put in the de-embed component?
It is difficult to answer without knowing what your problem and goal is.
If the connector is good, it will just add a phase delay. How much ... depends on the ref plane that you choose.