Hello,
I am using the Handheld Meter Logger software with a U1272A. I have a current clamp probe connected to the meter and am using the SCALE function in the meter. I have also enabled the NULL feature as well.
The meter displays the desired units (A) even though the rotary switch is in the mV position. And the NULL feature has removed the noise. However, when logging with the PC software it shows mV for units and the raw data, not the data displayed on the meter display. Is there a way to change that in the Meter Logger software?