AnsweredAssumed Answered

E36102B Labview Driver Error -108

Question asked by pius.k on Mar 16, 2020
Latest reply on Mar 18, 2020 by pius.k

Hi

 

I'm using a new E36102B power supply and getting error -108 "parameter not allowed" when I'm trying to enable the output with Labview.

I can set the voltage and current limit, also initialize and close is working.

But the "Configure Output Enabled.vi" fails all the time.

I can switch the output on manually.

 

I have installed:

E36xx, E36xxx DC Power Supply IVI and MATLAB Instrument Drivers 

Current Version: 1.6.1.0 | 2019-11-27

E36xx LabVIEW Driver for the Keysight Programmable Power Supplies

Current Version: 1.0.1 | 2019-08-13

also the Keysight IO Libraries Suite is installed, but I'm using NI MAX.

 

The power supply has the current firmware:

Current Firmware/Software

Version:1.0.1-1.00
Release Date:2017-08-28

 

I was able to set to output on with SCPI command: OUTP ON\n

This would be my only workaround to use directly the SCPI commands for all settings.

 

The vi which I downloaded uses the function AgE36xx_ConfigureOutputEnabled from the DLL AgE36xx**.dll

 

Does anyone have the same error, or may be gives me a hint?

Outcomes