I am using a 34903A to control a bank of valves (open, closed), while logging flow and pressure data with a 34901A. I need the state of the switches from the 34903A to be logged in the data file. The checkbox in the "configure channels" tab of BenchVue (DAQ app) for the "scan" column, is greyed-out (circled blue in the graphic). It does not appear that I can log the switch state from the options presented in the GUI. Is there another way to do this?
Thanks in advance,
Chuck