I would request to have a feature built in, similar to that which is implemented in the DAQ Benchvue Software, where upon clicking the "Stop" logging button, the data is automatically exported to your pre selected export directory. This has various benefits for the end user.
While making this request, i would additionally request options to set static Y axis values for viewing the data collected. This app likes to auto scale all the time, and does not appear to allow for the user to be able to pre-define axis scaling to provided the end user with the best view of the data being collected, and for consistent viewing format of the data.
Thanks
I moved this request to the BenchVue discussion so the people why normally monitor that will see your request when they gat back to work. And I'll ask the moderator to forward it to the software developement team to make sure they see it.