AnsweredAssumed Answered

external source control

Question asked by myonezaki on Jan 4, 2011
Latest reply on Jan 17, 2011 by odanzy
i have an external synthesize (psg) connected via gpib to an older pna (8362) and would like to control the power level via com.  from the pna, the external source (MySourcepsg) is available and is controlled from the power and attenuator pulldown.
1. is it possible to control the psg via com?
2. what is/are the commands to set the power level of the external source (ie. chan.testpower(1)=5dBm?)  

Outcomes