I cannot find a way to connect a standard 4mm banana cable to the front binding posts of the 30V/20A power supply, model E36233A.
There seem to have been designed to accept only large wires. How can i use my banana cables ? They are 20A rated.
Thanks,
Adrien
Adrien, that model comes with binding posts not banana jacks. All other 2-channel models with lower output current are banana jacks. You’ll either have to clip off the banana connector on one end or make new cables with stripped wires on one end. Not all banana cables support 20A so I suspect this was likely a safety consideration, especially if you combine current capacity from 2 channels which could be 40 A. The E36231A has banana plugs but only a single channel so current will be limited.