AnsweredAssumed Answered

Frequency Setup Overwrite of Sweepers While Using mmW Module

Question asked by jackzhu on Jan 2, 2020

Recently I need to test an E band device. I bought a Sage 4multiplexer, I use 8757D and 83623A. Since the source module is not made by HP/Agilent. It won't be recognized immediately by 8757D.

 

We had a 8350B in the past. We can use "shift" key and  then "start frequency", the number "4" and "s". After that, I can use "start frequency" and "stop frequency" to setup your operating frequency.

 

How can I do it similar in 83623A? I couldn't find this function from the manual. 

 

I greatly appreciate if anyone can help me to solve the problem to set up right frequency display on the 8757D. Thanks

Outcomes