I am using a N5244B and trying to collect data from a Noise Figure measurement remotely. I have set up the custom noise figure channel using CALC:CUST:DEF, DISP:WIND:TRAC:FEED, and CALC:PAR:SEL similar to examples that i have seen, and the result of CALC:PAR:CAT? is "noiseFig,NF" but have not been able to collect data from a Noise Figure measurement remotely.
Adding onto this, I am curious if there would be a way to set up two windows (one with s-parameters, the second window with a Noise Figure measurement) which is easily done from the front panel, but to do this through remote access, or even if the two windows are setup as a saved state, how would you access both the S-parameters and noise figure measurements. Allowing to remotely query each measurement separately.