AnsweredAssumed Answered

Errors in ADS show "X1 is an instance of an undefined model, cell_7" and "The instance `X1' has 4 pins, but the view `ECE262Project_lib:cell_7:schematic' has 0 pins."

Question asked by Yu-Tao on Nov 22, 2019
Latest reply on Nov 25, 2019 by Yu-Tao

Hi all:

 

I am simulating a square loop antenna, as the cell_7 in the attached rar file.

 

My structure consists of a primary loop with a capacitor and a secondary feeding loop for impedance matching.

 

Problems showed when exporting my design from ADS layout to schematic.  

 

The errors indicated "X1 is an instance of an undefined model, cell_7" & "The instance `X1' has 4 pins, but the view `ECE262Project_lib:cell_7:schematic' has 0 pins."

 

I've already run the simulation in the layout and it seemed fine. Both emModel and emSetup were built in the cell_7. 

I checked "Auto-update now" in the "Model" in the emSetup as well.

 

Both errors are still there although I googled and tried all the solutions in this forum.

 

I would appreciate whoever spends their time and patience in solving my problems.

 

Best regards,

Yu-Tao

Attachments

Outcomes