So I have used VEE to talk to many devices, mostly serial ones. Now I am trying to find out if I can use it to talk to a device via SNMP. But to be honest, I have no clue where to start. My experience with SNMP is limited to using MiB Browsers.
I am using Windows 10 and Vee 9.33
Any help and guidance would be greatly appreciated.
Thank you
You can launch windows CMD in VEE, telnet to the IP address of the device and then send your SNMP commands. Or you can use the socket function to input the SNMP commands once the port is configured correctly.
Scott
Sent from my iPhone