AnsweredAssumed Answered

E8363B LAN VISA usage.

Question asked by zubairrafiq on Oct 14, 2011
Latest reply on Oct 17, 2011 by jvall
I am using E8363B PNA series with Firmware A.06.32. What exactly I need to use LAN communication with my previously written SCPI commands for GPIB interface. Some of the commands are not working in matlab while using tcp-ip communication.
I failed to open VISA(visa-tcpip) properly (probably best solution for me ). I don’t know exactly my mistake is ? Detailed are attached below please suggest me what I should do?


This visa address is provided by Agilent IO libraries V 15.5.
>>Handle_pna=visa('agilent','TCPIP0::192.168.2.3::5025::SOCKET::INSTR')
??? Error using ==> visa.visa
Invalid RSRCNAME specified. Type 'instrhelp visa' for more information.


This works but cannot be opened.
>> Handle_pna =visa('agilent','TCPIP::192.168.2.3::INSTR')
>> fopen(Handle_pna)
??? Error using ==> icinterface.fopen
Could not open VISA object. Use INSTRHWINFO for a list of available configurations.


This works but I cannot send all commands properly while using matlab.

>>Handle_pna = tcpip('192.168.2.3', 5025)
>> fopen(Handle_pna)  

Outcomes