Hello
I have a 33512B which can perform square wave frequency sweeps. When I try to create the same waveform (square wave frequency sweep) with the Bench Link Waveform Builder Pro I can't see how to do it. I can only set sine wave.
In the end I need an externally triggerable sequence of two square wave sweeps with different frequency change rates to simulate a change in acceleration of a pulse generator.
Any kind of help is welcome!
Thanks