I am trying to export my layout to a symbol and simulate it in a schematic. The attached screenshots show the layout and its S11. I export it to a symbol and try to use it in a schematic, but the schematic simulation result does not match the layout simulation result.
Attached is the workspace where I fixed your mistake. The "test" testbench gives correct results with the attached workspace.
Your mistake is that the cell requires an emModel view that holds the EM simulation result, and must not have a schematic view. The testbench must be in another cell.
To create the emModel view, open the emSetup view and go to the model tab. There, you can create an emModel view, and make sure it is updated when you launch EM simulations manually.
The emModel view is the container that holds EM simulation results. If you have both schematic view and emModel view, it get's more complicated. I will skip that case here, because you don't need a schematic in your 0002L cell. The testbench must be in another cell.
I also made a few changed to your emSetup settings: solver RF mode is sufficient and much faster, adaptive sweep instead of discrete frequencies.
Best regards
Volker