AnsweredAssumed Answered

IO Libraries Suite Windows 10 Installation Issues

Question asked by JacoEngelbrecht on Oct 25, 2019
Latest reply on Dec 11, 2019 by vinathan

Hi, is anybody else experiencing issues with installing IO Libraries Suite on Windows 10? I tried several versions including 2019 Update 1 (IOLibSuite_18_1_24715.exe) and got a range of error messages as can be seen in the attached PDF. 

 

I have tried installing with the Windows Virus and Threat protection disabled but it made no difference. There is no other virus guard installed on this PC. The PC all the latest Windows 10 updates installed.

Outcomes