AnsweredAssumed Answered

PNA Leveling Mode via SCPI

Question asked by andyTPE on Sep 21, 2011
Latest reply on Sep 21, 2011 by gfarrel
Hello,

I have a PNA-X with 9.33 firmware.

I would like to be able to set the source leveling mode via SCPI.  From the UI I have the choices of:
Internal | Open Loop | Receiver - Rx

I can query the available modes using SOUR:POW:ALC:MODE:CAT?

This returns "INTernal,OPENloop,RxLeveling"

If I use the command SOUR:POW:ALC:MODE INT or SOUR:POW:ALC:MODE OPENLOOP, all is good.  However, I get an error from the analyzer if I try and set SOUR:POW:ALC:MODE RXLEVELING

I checked the 09.42 help file entry and it is the same as that for 09.33 for this topic.

So, bottom line question - how do I set the source leveling mode to RXLEVELING option

Thanks

Andy  

Outcomes