AnsweredAssumed Answered

How do I send ASCII to an 8 bit BRAINBOX I/O controller via IP? The command "#01000F" is ASCII. Prefix= "#". I/O Chan.= "01". Bit command= "000F". It's not working. Please help.

Question asked by eddbenson on Sep 19, 2019
Latest reply on Sep 20, 2019 by Stan Bischof

The Image is of my VEE short program with a To/From socket with my IP address for HOST NAME and ASCII code in a text box.This photo is showing I have the BrainBox I/O controller set up correctly in the Agilent Connection Expert.

Outcomes