AnsweredAssumed Answered

How to generate binary pattern with the 33522B Waveform Generator

Question asked by Waves905 on Sep 10, 2019
Latest reply on Sep 16, 2019 by Waves905

I was wondering how I can generate user defined pattern ex) 11101001 with  +/-5V for X amount of seconds  and 0V for X amount of seconds. How can I set a bit pattern using the waveform generator? Am I suppose to load like .txt or excel file with the pattern I want to the waveform? If so are there any examples of how one should format the file? Thanks.

Outcomes