AnsweredAssumed Answered

E5071C - Loading Error terms to ENA

Question asked by cav1783 on Aug 7, 2011
Hi,

i tried to perform load the error terms using the command below. but i encounter error "missing parameter" once i execute the second line. is there any missing command inside?

":SENS1:CORR:COEF:METH:SOLT1 1"
"SENS1:CORR:COEF ED,1,1,1,1E-20,1,1E-24"

tried to refer to the example
http://ena.tm.agilent.com/e5061b/manual ... icient.htm

but still doesnt help.  

Outcomes