Good hey,
I'm currently having an issue measuring power in LIST mode
as follows the routine of SCPI i follow and the result output i get and what i'm expecting to receive
- *RST
- SWE:POIN 11
- SWE:DWEL 1.5
- POW:MODE LIST
- POW:STAR 0
- POW:STOP 10
- INIT:CONT ON
after running this sequence of commands the display will now step through the power from 0-10 dBm
however the result from using the "POW:AMPL?" query will return -1.44E+002 (-144)
I'm expecting the output to return somewhere within the range of 0,+10
Firmware version B.01.65
If this is not the correct procedure please give some guidance on how to proceed
Regards
John