AnsweredAssumed Answered

Lynx3dm tab missing

Question asked by DavidC on Aug 6, 2019
Latest reply on Aug 6, 2019 by jvall

Setting up a used PNA for external Monitor display the Lynx 3dm+ tab is missing.

On the Keysight PNA and PNA-L Series of Network Analyzers, what are the hot keys to set-up the various internal and exte… 

The PNA Display adapter is stated as the Silicon motion Lynx 3dm+ driver.

Looking at other PNAs with the same display adapter it running the same version of the drivers 6.13.1.263. Is there a setting that can be changed to bring the tab into advanced settings , or need to try to reinstall the display driver?

Outcomes