AnsweredAssumed Answered

Why can't I load an intrsument State to the DAQ App, or load from an existing data log?

Question asked by rodtheintern on Jul 17, 2019
Latest reply on Jul 26, 2019 by rodtheintern

Regarding the DAQ application, I have used this Benchvue app with the 34972A for the past 3 years. For the first time, I am seeing an error when attempting to load an instrument state to the device after connecting it via USB. I haven't tried over ethernet yet. But I build up a state, save it, and cannot load it again. I also cannot load from a previous data log either. I get the error: “AppInstance: LoadConfigFile. – Error Occurred. Error Code : -8004” and “AppInstance: LoadConfigFile. – Error Occurred. (BenchVueExceptoin type):” w0dz

Attachments

Outcomes