AnsweredAssumed Answered

Can I create a LTE Systemvue project with only one UE, resource allocation type 1. The result CRC pass in VSA decode

Question asked by thangtv8 on Jul 16, 2019

Hi Specialist,

 

I come from Vinsmart Company. I'm trying to use Systemvue to create the Reference Testvector for my RRH in LTE Project.

 

So I create a project having only one UE, resource allocation type 1. But my result alway CRC Fail in almost subframe (as my picture). As I see, the pdcch data from Systemvue always not full the Symbol for pdcch. But if I create this testcase in Signal studio, pdcch always full all symbol for pdcch. Is that the fault of system vue ? Please help me. Thank you so much.

Attachments

Outcomes