I'm running Genesys 2014.03(x64) and I accidently deleted my workspace tree. Now I can't get it to show up. I go to View and check Workspace Tree but it doesn't show up whether it is checked or unchecked. How do I fix this?
I'm running Genesys 2014.03(x64) and I accidently deleted my workspace tree. Now I can't get it to show up. I go to View and check Workspace Tree but it doesn't show up whether it is checked or unchecked. How do I fix this?
I have tried both and it doesn't show up. If it was that simple I wouldn't have to ask. I had the problem a while back and then it started working. Not sure why. The problem has come back. I'm running three monitors so maybe Genesys is getting confused? Anyone else seen this problem? How do you recover? It's both the workspace tree and tune. Neither one shows up.
Hi,
if auto hide is selected, the workspace tree is not visible, but on left.
If so, then press this tab, then move the cursor to the window bar and choose auto hide off. If you have multiple screens, then put the floating window and you can move it to the screen you prefer. Same thing for tune windows.
Yves
This isn't the problem. Here's a screen shot. I clicked around the boundaries of the main window and Sch1 and neither have anything hidden.
workspace is checked. Also tried key presses and same for Tune. Neither of them shows. If I remember Tune and Workspace tree are the same window but with tabs. Nothing showing on my other displays. When you press "Hide" do you still get the tab on the left?
Have you try F7 key ?
I tried to cause the problem without success: I added another monitor moved all the windows, opened all the toolboxes. Open, close the software, make a video link break on the second monitor ... I always end up reactivating the workspace tree in one way or another.
Yves
Hi, on top menu VIEW, check for Worspace Tree or CTRL+SHIFT+W (toogle command)
Yves