Hi, this is pin out for my 33322H 0-110dB, but 40dB step is replaced by 30dB step for max 90dB (33323K) instead of 110dB. I suppose this pinout will be good if you have same connection type. If not same connection type, see chart below from pdf (see link)
Hi, this is pin out for my 33322H 0-110dB, but 40dB step is replaced by 30dB step for max 90dB (33323K) instead of 110dB. I suppose this pinout will be good if you have same connection type. If not same connection type, see chart below from pdf (see link)
33323K attenuator
Yves