Hello
My configuration is N5247B-423 + N5292A + VDI mini module extender for WR6.5.
The error message "-224 Illegal parameter value" pops up after I upgrade the firmware to version A.13.60.06
I can't fix it even I reboot or preset PNA or even re-install firmware.
This error messege shows only under millimeter-wave mode.
It never occurs when it's on Standard PNA mode.
What should I do to fix this problem? Thank you
I just spotted this question, is it still an issue? Did this work before on an older version of firmware? It is likely some issue in the cached data for the mm-mode that is not consisted with the new firmware. I know there is such a cache but I don't know where it is located for sure. I think you will find it in C:\ProgramData\Keysight\Network Analyzer\Configurations Note ProgramData is hidden so you have to show hidden files to see it. Try copying all the configurations to a new folder on the desktop (in case you need to get them back) and then deleting everything. Mind you, I don't know that this will work but it's my best guess.