Hi , I'm Trying to configure the N5172B MXG with a Configuration consisting of only DCI0 with NDI as 1 and TPC bits as "1" for a RNTI 65 with iMCS4 and NumPRB 4 for computing the RIV bits. This signal is generated and visualized on the MXA N9020A and found that all SubFrames are not decoding as DCI0 Signal on PDCCH chanel.
When I'm making TPC bits as Zero all the SubFrames are decoding correctly.
Is there any known Issue in the Software .