AnsweredAssumed Answered

Channel.DoResponseCal

Question asked by andeezlemoyo on Jun 13, 2019
Latest reply on Jun 13, 2019 by daras

I'm using N5247A with the latest firmware, DCOM.  IChannel22 and ICalibrator10 interfaces.

when I call the DoResponseCal method of the Channel class, I get this error: Method DoResponseCal failed: The operation was canceled.

But that doesn't make any sense, nothing was cancelled.

The channel is a standard s-parameter measurement and if I do a response cal manually using the PNA firmware it works fine. But I need to launch the response calibrator remotely through my software.

Any ideas or a working example?

Thank you!

Andy

Outcomes